2015-07-27 7:23 AM
Hi,
When the SPWF01 is in miniAP mode what setup will allow the client to resolve the module's domain name. Do I need to set ip_dns to be the module's IP address ? Thanks, Mark2015-07-27 8:13 AM
Hi Mark,
variable called ''ip_use_dhcp'' enables miniAP to run both dhcp and dns server feature. Clients (up to 5) can ask for ''ip_apdomainname'' resource, and miniAP can resolve that address to IP address.jWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.