2019-11-29 1:29 AM
I would like to add a TMR interrupt to manage an action every 1sec.
Code used now in the stm32746g_discovery.c file:
void TIM2_IRQHandler(void)
{
if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
{
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
STM32vldiscovery_LEDToggle(LED3);
}
}
void BSP_TIM2_Init()
{
TIM_TimeBaseInitTypeDef TIM_StructInit;
NVIC_InitTypeDef NVIC_StructInit;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
TIM_StructInit.TIM_Period=Period;
TIM_StructInit.TIM_Prescaler=Prescaler;
TIM_StructInit.TIM_ClockDivision=TIM_CKD_DIV1;
TIM_StructInit.TIM_CounterMode=TIM_CounterMode_Up;
TIM_StructInit.TIM_RepetitionCounter=0;
TIM_TimeBaseInit(TIM2, &TIM_StructInit);
TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
TIM_Cmd(TIM2, ENABLE);
TIM_ClearFlag(TIM2, TIM_FLAG_Update);
NVIC_StructInit.NVIC_IRQChannel=TIM2_IRQn;
NVIC_StructInit.NVIC_IRQChannelCmd=ENABLE;
NVIC_StructInit.NVIC_IRQChannelPreemptionPriority=0;
NVIC_StructInit.NVIC_IRQChannelSubPriority=1;
NVIC_Init(&NVIC_StructInit);
}
errors:
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c: In function 'TIM2_IRQHandler':
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c:379:7: warning: implicit declaration of function 'TIM_GetITStatus' [-Wimplicit-function-declaration]
if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
^~~~~~~~~~~~~~~
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c:379:29: error: 'TIM_IT_Update' undeclared (first use in this function)
if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
^~~~~~~~~~~~~
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c:379:29: note: each undeclared identifier is reported only once for each function it appears in
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c:381:5: warning: implicit declaration of function 'TIM_ClearITPendingBit' [-Wimplicit-function-declaration]
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
^~~~~~~~~~~~~~~~~~~~~
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.