cancel
Showing results for 
Search instead for 
Did you mean: 

What additional fees / Bluetooth SIG fees apply to any development I do with BlueNRG-355MC SOC?

JWill.8
Associate III

I am hoping this has a simple answer. If I develop a solution based on the BLUENRG-355MC and attribute that design is based STMicroelectronics SOC solution, are there additional fees I need to be aware of?

I checked the following link:https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/ and saw that this https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/ SOC was qualified with Bluetooth SIG.

Would I be subjected to additional fees from Bluetooth SIG?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Laurent LOUAZON
ST Employee

Hello,

True our BlueNRG-355 is certified (stack and PHY) at BT SIG alliance.

Now, all products using Bluetooth must complete the Bluetooth Qualification process (it is a licenced technology belonging to Bluetooth SIG).

If using a SoC (such as BlueNRG 355), you must complete :

  • RF testing (around 10k$ from a BQTF - Bluetooth Qualification Test Facility)
  • Product listing (also around 10k$)

Please note

  • this is valid whatever BLE manufacturer you will use
  • When using a full integrated module (BLE SoC + xtals+antenna etc) having a end product certification, you will "only" have to consider product listing (as module is end product RF certified)

Regards

Laurent

View solution in original post

2 REPLIES 2
Laurent LOUAZON
ST Employee

Hello,

True our BlueNRG-355 is certified (stack and PHY) at BT SIG alliance.

Now, all products using Bluetooth must complete the Bluetooth Qualification process (it is a licenced technology belonging to Bluetooth SIG).

If using a SoC (such as BlueNRG 355), you must complete :

  • RF testing (around 10k$ from a BQTF - Bluetooth Qualification Test Facility)
  • Product listing (also around 10k$)

Please note

  • this is valid whatever BLE manufacturer you will use
  • When using a full integrated module (BLE SoC + xtals+antenna etc) having a end product certification, you will "only" have to consider product listing (as module is end product RF certified)

Regards

Laurent

JWill.8
Associate III

Hi Laurent,

Thank you very much for this information.

Jeff

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.