2023-02-22 12:20 AM
Hello.
I want to get the results through unicleo-gui using the sensortile kit.
I soldered sensortile to the cradle.
Before soldering the sensortile to the cradle, I connected it to the expansion board and checked that it was connected to the mobile phone application by Bluetooth.
When connected to the computer usb line, the red light keeps turning on when the cradle is switched on, and when the switch is turned off, the red light blinks quickly.
I want to connect with the computer's unicleo-gui while the computer's USB line and cradle are connected.
However, as things stand, the computer and sensortile(soldered with cradle) are not connected via Bluetooth.
Is there anything I can do now?
Do I need to install firmware or is there another problem?
If I need to install firmware, can you explain the detailed method?
I've been thinking about this for quite a while.
I'd appreciate it if you could let me know.
Thank you for reading it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.