2024-08-01 11:32 PM - last edited on 2024-08-02 1:52 AM by Peter BENSCH
Hi everyone,
I met a problem when I measured the current rms value with stpm33 ic.I'm using this IC with resistive loads and other load profiles with low crest factor. But I met a case with a high crest factor load like as SMPS type loads.
I collected the momentary current datas from STPM33eval board over SPI lines. And than calculate the RMS current value using with point by point datas. The calculated value asme as real value. I compared the calculated value with true RMS values that are measured with other power analyzers as called as Vitrek PA900 and Schneider PA module.
I compared the current values with resistive and refrigerature type loads. They are same for all measurement device.
Is it possible to make any mistake when I config the STPM?
You can find my measured values and voltage-current graph at below.
Blue: Actual Voltage Orange: Actual Current
| Load | STPM33 Current RMS(mA) | STPM33 Current Calculated RMS(mA) | Vitrek PA900 RMS(mA) | Scheneider PM2200 RMS(mA) |
| High Crest Factor SMPS Load | 119,9 | 199 | 198 | 198 |
| Low Crest Factor Load (Resistive Load) | 1033 | 1033 | 1033 | 1033 |
2024-09-25 3:36 AM
Hi again,
I opened a ticket explaining my issue for this error. However, the STM team stated that it’s not possible to resolve this issue with the STPM33. They pointed out that the reason is due to the current signal having a high peak. Based on their recommendation, I should handle this with raw data. But this is not possible with my design, as I am using UART communication. I didn’t expect an IC that performs RMS readings to make such a fundamental error. If I have to perform RMS and all other calculations with raw data, I don't fully understand how the STPM differs from an ADC with a high input voltage.
2025-04-14 11:42 AM
Hi bsahan,
I would like to know if you were able to solve this problem.
I am working on a meter that must meet class 0.2 measurements, and the main loads will be SPMS converters.
I inserted this chip into the project with the greatest confidence because it is from a manufacturer like ST, and I never expected that there could be such a grotesque error in the component.
Please, if you managed to find a solution to your problem and it is possible, share it with me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.