2021-03-08 8:02 AM
Hi everyone, I am new for STUSB4710A. I connect STUSB4710a STEVAL_ISC004v1 evaluation board to my laptop, through a min b usb cable. when I run the graphic interface en.stsw-stusb001, there is one error: usb error: no target found. please connect first the evaluation board with a usb cable. I powered on / off the device. The software still does not find the STUSB4710A. shall install some drivers? Thanks.
Solved! Go to Solution.
2021-03-09 6:47 AM
Let's make a little clearer about what you need to do:
Good luck!
/Peter
2021-03-08 8:13 AM
Did you read the UM2254 (STSW-STUSB001 quick installation guide)?
The introduction says:
In order to run the GUI on a laptop, an STM32 Nucleo board must be programmed to act as a USB to I²C bridge between the laptop and the STUSB evaluation boards.
Good luck!
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
/Peter
2021-03-08 8:22 AM
2021-03-09 4:57 AM
Hi, peter, sorry to disturb you again. Yes, from the beginning, I followed the manual, according to the manual, if I connect STUSB4710A to my laptop through a usb min b cable, the windows system should install the driver. This is written at the step 2. But I tried several computers, 2 usb cables, 3 STUSB4710A boards(we bought 6 ST products.) But each time when I connect the STEVAL_ISC004v1 evaluation board, no any response in my windows system. So maybe I can not programm STEVAL_ISC004v1 evaluation board. But according to the manual for STEVAL_ISC004v1 evaluation board, I should be able to do this. Could you have a look ? thanks a lot. As a summary, step 2 in the manual does not work for me
2021-03-09 6:47 AM
Let's make a little clearer about what you need to do:
Good luck!
/Peter
2021-03-10 2:43 AM
Hi Peter,
Thank you so much. Indeed, I was wondering it should have not been so complex. Yes, I misunderstood something. Thanks again.
2021-03-17 3:26 PM
Hello,
There may be some confusion because the STUSB4710 GUI v3.2.3 requires 2 USB cables:
- one USB-mini cable (connected to STM32 Nucleo board)
- one USB-micro cable (connected to STUSB4700 eval board)
This can make the setup complicated.
An alternative is to use the GUI v3.5 which only needs 1 USB-mini cable (connected to STM32 Nucleo board).
You can download it here:
https://community.st.com/s/question/0D53W00000HySKa/stusb4700-gui-offline
2025-04-14 1:17 PM
Thanks for you assistance! Four years later and you have resolved my issue. I responded on my thread showing your response as I am sure it will help other members. FYI... GUI v3.5 is not even on the ST website, they are still showing the v3.2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.