2020-11-26 2:23 AM
Hi everyone, I'm working on a project where I interface the micro STM32F746ZGT6 with a CMOS sensor to acquire images. What I wanted to do is then transmit them using an HDMI connector but I don't understand which communication pins of the micro I could use. I only find an HDMI-CEC for control, nothing for parallel transmission. Any solution?
2020-11-26 2:55 AM
The STM32 do not provide an HDMI port, so an adapter interface is necessary.
Some STM32 (e.g. STM32F769, STM32H747) contain a peripheral called MIPI-DSI for which an adapter from DSI to HDMI is available: B-LCDAD-HDMI1.
Good luck!
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-11-26 5:05 AM
VGA might be feasible if all the LCD pins are available in the design.
The F769 or F469 would have been better part choices to get to HDMI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.