2017-05-28 10:54 PM
I want to convert the currently converted microphone data to BLE, and store the data in STEVAL-IDB006V1M Dongle to PC. (To convert wav file)
The STM32L432KC and BlueNRG-MS were used to convert the analog microphone data to digital and send the digital data to the BLE.We then connected the STEVAL-IDB006V1M Dongle to the PC and confirmed the BLE Data sent to the BlueNRG GUI software.However, we only showed data one by one in real time, and we could not find the function we wanted in the GUI program.The question is.
If you do not have the ability to store BLE Data separately sent in real time from the BlueNRG GUI program, I wonder if there is other software of ST that supports this function.
STEVAL-IDB006V1M I want to save the BLE data received from the PC in Dongle in TEXT file or WAV file format in real time, but I could not find any format for it.
Please do not hesitate to contact us by e-mail.
Thank you.
2017-05-30 3:37 AM
Dear Jang Insang,
for your use case, you may be interested in the
software package.It has two parts:
the application is responsible for the decompression of ADPCM audio data received via BLE and for USB streaming of decoded PCM samples.
This package is based on ST's MEMS digital microphones. IT doesn't support your STEVAL-IDB006V1M dongle out of the box, as it is available for STM32 Nucleo board with X-NUCLEO-IDB05A1 (BLE expansion board based on the same BlueNRG-MS module of STEVAL-IDB006V1M) and X-NUCLEO-CCA02M1 (MEMS microphones expansion board).
Hope that helps,
Antonio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.