2019-02-26 12:37 PM
Hello.
I want to decrease power consumption of Steval-FKI433V2 and to cut ST-Link PCB part, but later.
Conditions:
If JP5/pins2,3 are shorted: Nucleo, S2-LP and ST-Link are powered, the Steval works properly (it sends back received data) but the consumption is changed between 52mA and 65mA and two-colored LED is blinking approx. once per second.
If JP5 pins are not shorted and 3V7 battery is connected to CN7/pin18(+5V), only Nucleo and S2-LP are powered (ST-LINK is not powered). The consumption is 20mA, but device doesn't work.
As ST-Link's uC is not powered, too small voltage is present in the NRST net, I pulled it up to 2V85, but device doesn't work.
I see also, that when powered, ST-Link provides 8MHz to Nucleo's uC (MCO net), but in SDK_Chat.c HSI oscillator is selected, so external 8MHz should not be used.
Question: what else should I do to power only Nucleo and S2-LP now, when ST-Link is not cutted and should not be supplied with power? May be some special changes in SDK_Chat.c program must be done?
2019-02-27 1:41 AM
I've solved the problem.
In SDK_Chat.c remove the string '#define USE_VCOM' (place delimiter '//' before it):
//#define USE_VCOM
3V7 battery:
'+' is connected to CN7/pin18 or CN6/pin5 (+5V); '-' to CN7/pin20 or CN6/pin6 (GROUND);
JP5 (3 pins): jumper is removed;
R=1k: between CN6/2(+3V3) and CN6/3(NRST) (If ST-Link part of PCB would be cut, R may be increased up to 4k7...10k);
3V7 consumption: 18mA, when green LED is off, 20mA - LED on.
To decrease the consumption,
remove the strings 'SdkEvalLedToggle(LED1);' in SDK_Chat.c (green LED off, consumption 18mA):
remove R32 (red LED off, consumption 16mA).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.