2026-02-23 1:52 AM
Hello,
I've got a question about pairing and bonding for BLE with iOS devices for ST67W61.
I've checked available functions and AT commands, I don't see any mean to encrypt the characteristic. As the iOS BLE stack requires it to pair and bond - am I missing something or it's not yet implemented?
Best regards
Solved! Go to Solution.
2026-03-06 3:59 AM
Hi @Shirovaty
I confirmed internally that the ST67 defaults to bonding. There is no flag implemented to select between pairing and bonding. I asked R&D to look into this topic, and I will update this post when there is news.
Best regards
2026-02-27 12:39 AM
Hi @Shirovaty
I confirm that this feature is not available.
The BLEGATTSCHARCRE AT command can be called with char_perm set to read permission or write permission. This allows the remote device to access the characteristic without encryption.
By performing authenticated pairing, it is possible to encrypt the characteristic or data. You can replace the missing feature by requesting pairing automatically after the connection event. Does this solution meet your requirements?
Best regards,
2026-02-27 12:54 AM
Hi @TarikAb,
I've came across this solution (using securityStart() at connection) but there is another issue linked to it.
For some reason both iOS and Android default to bonding instead of pairing, which is problematic in terms of iOS - unbonding is tedious on this OS.
BLE Specification mentions Bonding Flag in the pairing request, which is responsible for indicating if the request is for pairing or bonding. Is there any option to set it from x-cube-st67w61 or AT commands?
Thanks for your help!
2026-03-06 3:59 AM
Hi @Shirovaty
I confirmed internally that the ST67 defaults to bonding. There is no flag implemented to select between pairing and bonding. I asked R&D to look into this topic, and I will update this post when there is news.
Best regards
2026-03-06 4:04 AM
Hi @TarikAb
Thanks for the info, for now it's not such a problem, but this update will come in handy in future :)
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.