2017-01-24 5:13 PM
My application receives data in usart1 and usart2 through interrupt.
I generated the files in STM32CubeMX for keil.This error appears in the compilation:../Src/stm32f1xx_it.c(193): Error: # 20: identifier 'USART_IT_RXNE' is undefined.How do I solve this?Void USART1_IRQHandler (void)
{ If (USART_GetITStatus (USART1, USART_IT_RXNE)! = RESET) // enter interrupt when STM32 receice data. { USART_Temp_Data = USART_ReceiveData (USART1); }}void HAL_MspInit(void)
{ /* USER CODE BEGIN MspInit 0 *//* USER CODE END MspInit 0 */
__HAL_RCC_AFIO_CLK_ENABLE();
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* System interrupt init*/
/* MemoryManagement_IRQn interrupt configuration */ HAL_NVIC_SetPriority(MemoryManagement_IRQn, 0, 0); /* BusFault_IRQn interrupt configuration */ HAL_NVIC_SetPriority(BusFault_IRQn, 0, 0); /* UsageFault_IRQn interrupt configuration */ HAL_NVIC_SetPriority(UsageFault_IRQn, 0, 0); /* SVCall_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SVCall_IRQn, 0, 0); /* DebugMonitor_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DebugMonitor_IRQn, 0, 0); /* PendSV_IRQn interrupt configuration */ HAL_NVIC_SetPriority(PendSV_IRQn, 0, 0); /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);/**DISABLE: JTAG-DP Disabled and SW-DP Disabled
*/ __HAL_AFIO_REMAP_SWJ_DISABLE();/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{GPIO_InitTypeDef GPIO_InitStruct;
if(huart->Instance==USART1) { /* USER CODE BEGIN USART1_MspInit 0 *//* USER CODE END USART1_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART1_CLK_ENABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ GPIO_InitStruct.Pin = GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* Peripheral interrupt init */
HAL_NVIC_SetPriority(USART1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART1_IRQn); /* USER CODE BEGIN USART1_MspInit 1 *//* USER CODE END USART1_MspInit 1 */
} else if(huart->Instance==USART2) { /* USER CODE BEGIN USART2_MspInit 0 *//* USER CODE END USART2_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* Peripheral interrupt init */
HAL_NVIC_SetPriority(USART2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); /* USER CODE BEGIN USART2_MspInit 1 *//* USER CODE END USART2_MspInit 1 */
}}
void HAL_UART_MspDeInit(UART_HandleTypeDef* huart)
{if(huart->Instance==USART1)
{ /* USER CODE BEGIN USART1_MspDeInit 0 *//* USER CODE END USART1_MspDeInit 0 */
/* Peripheral clock disable */ __HAL_RCC_USART1_CLK_DISABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_9|GPIO_PIN_10);/* Peripheral interrupt DeInit*/
HAL_NVIC_DisableIRQ(USART1_IRQn);/* USER CODE BEGIN USART1_MspDeInit 1 */
/* USER CODE END USART1_MspDeInit 1 */
} else if(huart->Instance==USART2) { /* USER CODE BEGIN USART2_MspDeInit 0 *//* USER CODE END USART2_MspDeInit 0 */
/* Peripheral clock disable */ __HAL_RCC_USART2_CLK_DISABLE(); /**USART2 GPIO Configuration PA2 ------> USART2_TX PA3 ------> USART2_RX */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2|GPIO_PIN_3);/* Peripheral interrupt DeInit*/
HAL_NVIC_DisableIRQ(USART2_IRQn);/* USER CODE BEGIN USART2_MspDeInit 1 */
/* USER CODE END USART2_MspDeInit 1 */
}}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/**
* @} *//**
* @}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.