2017-06-11 11:38 PM
Hi,
is it possible to use a splitter to have two wifi antennas with the SPWF moduls?
One antenna would be in side the housing, the second antenna shall have a cable with 1m length, e.g.
http://www.teltonika.lt/de/product/wifi-antenna-5dbi-magnetic-type/
Using the modules u.fl connector and connect a cable with a SMA connector, then using a SMA splitter to connect the internal and the external antenna.
Are there any experiences about this?
BR,
Flow
2017-06-12 12:57 AM
2 antennas at the same time?
2017-06-13 12:20 AM
Sometimes - the second, external antenna shall be optional mountable to increase the range if the device is mounted in a steel box. So the antenna will be outside of this box...
2017-06-13 6:59 AM
You can mount 2 antennas, and use only one of them. Use a switch to select the antenna to use.
I'm not an RF expert, but I think cannot use 2 antennas at the same time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.