2017-12-07 7:02 AM
hi,
stm32F401RB + en.x-cube-wifi1_firmware_v3.0.2
SPFW04Sx + UART + FW1.1.0
in my code i use AT+S.FSP and i want to catch the USART_Receive_AT_Resp in the buffer.
My problem is that response doesn't give +WIND and i don't know how to process the response!
in wifi_module_uart_04.c i check Process_DMA_Buffer_Messages() message type is case OK:
/*Now Check to which AT Cmd response this OK belongs to so that correct parsing can be done*/
go to else
//This is a standalone OK
/*Cases possible - TLSCERT,TLSCERT2, TLSDOMAIN, SETTIME - S.SOCKW, SOCKR, S.SOCKC, S.SOCKD (open a server socket) - File Operations - S.GPIOC and S.GPIOW */I don't know and see what code i must add.
The goal is to put response in a buffer and manage it in the main.
thks
yoann
2017-12-07 7:30 AM
To continu:
when i run in the code
//main.c
status = wifi_file_print_content((uint8_t *) RootCertFileName);
Read_DMA_Buffer is call (void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
in the dma_buffer, i don't receive the beginning of the file. (lose the first 796 caractere for a total of 1322)
2017-12-08 4:58 AM
'To continu:
when i run in the code
//main.c
status = wifi_file_print_content((uint8_t *) RootCertFileName);
Read_DMA_Buffer is call (void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
in the dma_buffer, i don't receive the beginning of the file. (lose the first 796 caractere for a total of 1322)'
Buffer is circular so the complete response of the cmde AT+S.FSP is in the buffer. But whaqt is the good process to catch response!
i am trying to modify the Process_DMA_Buffer
/* Response Received..AT-S.*/ with test WiFi_Control_Variables.enable_receive_file_response
i will inform on my progress.
I hope i am in the good way/solution.
yoann
2017-12-11 2:49 AM
You can think about the IDLE interrupt over UART: when it fires, all data (between AT+S.command and AT-S.OK/ERROR) were printed, and final OK/ERROR was given (+ 'timeout').
Worst case: a '+WIND:something' has come after the OK/ERROR. In this case, IDLE interrupt follows the WIND, and not the OK/ERROR. But it's a simple case to manage.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.