2018-05-02 3:36 AM
I am posting data up to a server using HTTP post, the module sends the data in chunked mode. It is a relatively short packet, so is sent in one transfer. However the module does not end the transfer by sending a last chunk character, I.e. '0' therefore leaving the server expecting more data.
The module then closes the connection with FIN-ACK, yet leaving the server expecting more data, so obviously the server responds with an error on every post. Rather annoying!
Please fix or suggest how the chunked transfer can terminated correctly!
FYI:
3.6.1 Chunked Transfer Coding The chunked encoding modifies the body of a message in order to transfer it as a series of chunks, each with its own size indicator, followed by an OPTIONAL trailer containing entity-header fields. This allows dynamically produced content to be transferred along with the information necessary for the recipient to verify that it has received the full message. Chunked-Body = *chunk last-chunk trailer CRLF chunk = chunk-size [ chunk-extension ] CRLF chunk-data CRLF chunk-size = 1*HEX last-chunk = 1*('0') [ chunk-extension ] CRLF chunk-extension= *( ';' chunk-ext-name [ '=' chunk-ext-val ] ) chunk-ext-name = token chunk-ext-val = token | quoted-string chunk-data = chunk-size(OCTET) trailer = *(entity-header CRLF) The chunk-size field is a string of hex digits indicating the size of the chunk. The chunked encoding is ended by any chunk whose size is zero, followed by the trailer, which is terminated by an empty line. The trailer allows the sender to include additional HTTP header fields at the end of the message. The Trailer header field can be used to indicate which header fields are included in a trailer (see section 14.40).
2018-05-02 9:37 AM
Hello,
this is surprising to me...
However, I just tried to POST a form from a file containing 20 characters (direction=up&counter=2).
The command I used to send the form to my POST test server is:
AT+S.HTTPPOST=192.168.1.112,/post,5000,,,,,f.form
while the data captured by wireshark is:
00000000 50 4f 53 54 20 2f 70 6f 73 74 20 48 54 54 50 2f POST /po st HTTP/
00000010 31 2e 31 0d 0a 43 6f 6e 74 65 6e 74 2d 54 79 70 1.1..Con tent-Typ00000020 65 3a 20 61 70 70 6c 69 63 61 74 69 6f 6e 2f 78 e: appli cation/x00000030 2d 77 77 77 2d 66 6f 72 6d 2d 75 72 6c 65 6e 63 -www-for m-urlenc00000040 6f 64 65 64 0d 0a 48 6f 73 74 3a 20 31 39 32 2e oded..Ho st: 192.00000050 31 36 38 2e 31 2e 31 31 32 3a 35 30 30 30 0d 0a 168.1.11 2:5000..00000060 54 72 61 6e 73 66 65 72 2d 45 6e 63 6f 64 69 6e Transfer -Encodin00000070 67 3a 20 63 68 75 6e 6b 65 64 0d 0a 55 73 65 72 g: chunk ed..User00000080 2d 41 67 65 6e 74 3a 20 48 54 54 50 2d 43 6c 69 -Agent: HTTP-Cli00000090 65 6e 74 0d 0a 0d ent...00000096 0a .00000097 31 34 0d 0a 14..0000009B 64 69 72 65 63 74 69 6f 6e 3d 75 70 26 63 6f 75 directio n=up&cou000000AB 6e 74 3d 32 nt=2000000AF 0d 0a ..000000B1 30 0d 0a 0d 0a 0....then the server reply follows and the TCP connection is eventually closed by the SPWF04.
2018-05-02 9:57 AM
Hi Elio
Thanks for looking into this for me.
I have just repeated your findings and the terminator was present and CORRECT.
It seems certain content types are not sending the terminator. Up to press I have tried:
.html - NO Terminator
.fhtml - NO Terminator
.json - Terminator CORRECT
.form - Terminator CORRECT
I'm not sure about the others, but I think I can get around it by changing my content type now.
Thanks
Jonathan
2018-05-03 6:39 AM
Hi Elio
I can repeat it with several strings but below is a direct copy of the serial strings sent to the module.
Note, I have changed the delimiter to $ so as to support json format.
\' is just ' , the below is formatted to be put straight into a string with sprintf.
This fails:
AT+S.FSD=2:\\Upload.html\r
AT+S.FSC=2:\\Upload.html$108\r{\'uid\':\'230025001351363035343137\',\'model\':5000,\'token\':\'16293677d61b4b06face4c6db2de20efbb6d6188b8cd556613\'}\r\rAT+S.HTTPPOST=xxxxxxxxxx.westeurope.cloudapp.azure.com$/device/get_data_device/$3002$$$$$2:\\Upload.html\rThis works:
AT+S.FSD=2:\\Upload.json\r
AT+S.FSC=2:\\Upload.json$108\r{\'uid\':\'230025001351363035343137\',\'model\':5000,\'token\':\'16293677d61b4b06face4c6db2de20efbb6d6188b8cd556613\'}\r\rAT+S.HTTPPOST=xxxxxxxxxx.westeurope.cloudapp.azure.com$/device/get_data_device/$3002$$$$$2:\\Upload.json\rI also use wire shark and the terminator is clearly present when using json but NOT with html.
baud 115200, and no delay between sending the strings.
I don't believe anything else has changed from default.
Jonathan
2018-05-03 7:28 AM
Hello Jonathan,
maybe I'm not catching the point... I have saved the string abobe in file with several extensions (html, fhtml, jpg, ...): the Content-Type header is changed accordingly and the trailing 30 0d 0a 0d 0a is always present.
Am I doing the same as you?
Regards,
Elio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.