2016-08-18 9:41 PM
Hi,
I'm communicate two spwf01 module one as server and another one as client use AT commands. Client send data to server and on the UART rx interrupt is generating for the received data. But it sends data from server to client I'm not getting any indication of data arrival. How to solve this problem.
Kindly provide sever and client both way communication example AT command code.
please suggest to solve this issue
Thank you
Basavanagouda
2016-08-23 12:32 PM
Socket client: use '',ind'' parameter to SOCKON command to get an indication when something was received.
Socket server: automatically switches to data mode when something was received. Note that socket server has no AT commands. Use Hands-On manual to get some example2016-09-01 3:15 AM
Hi,
I observed followings while communicating between two Wi-Fi 4click modules:
At the Client side when its try to connect to server I’m using AT+S.SOCKON command to connect.
In this command I can pass “ind� parameter which can indicate data arrival at the client side with “+WIND:55:Pending Data� on UART interrupt .
Client side it is taking 500ms to receive WIND:55:Pending Data: interrupt.
Server to client data transmission it takes only 5 to 6ms.
Please suggest how to solve this time delay at the client side.
Thank you
Basavanagouda
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.