2015-08-13 4:38 AM
Hi everyone,
I'm using SPWF01SA.11 as a client in tcp connection but when i try to send escape_seq message getting ''ERROR: Data mode not available '' I'm wondering is there no data mode in tcp client connection? I get confuse little bit Thanks2015-08-13 5:34 AM
Hi,
socket client is always in command mode. Data mode is not available in this case. Data mode switch is available in case of socket server: when a socket client connects to module, the module itself automatically switchs to data mode. jerry2015-08-14 5:54 AM
2016-08-18 12:05 PM
Hi,
I'm using two SPWF01S module, I have configured one module as Access point act as server and another as a station (client) using AT commands(UART interface).
Client and server communication is happening client able to send data to server and I can see these data at the UART receive interrupt(I'm considering this as data arrival ).
But if I send data from server to client how I can know that data is reach to client.
Is there any indication or command to see data arrival?
If I Use read AT command to read the data, it will read and give UART interrupt but in client to server data communication without read command UART interrupt is coming.
How I can know sent data came to other end?
Please help me to solve this.
Thank you
Basavanagouda
2016-08-23 12:29 PM
Socket client: use '',ind'' parameter to SOCKON command to get an indication when something was received.
Socket server: automatically switches to data mode when something was received. Note that socket server has no AT commands.2016-09-01 3:16 AM
Hi,
I observed followings while communicating between two Wi-Fi 4click modules:
At the Client side when its try to connect to server I’m using AT+S.SOCKON command to connect.
In this command I can pass “ind� parameter which can indicate data arrival at the client side with “+WIND:55:Pending Data� on UART interrupt .
Client side it is taking 500ms to receive WIND:55:Pending Data: interrupt.
Server to client data transmission it takes only 5 to 6ms.
Please suggest how to solve this time delay at the client side.
Thank you
Basavanagouda
2016-09-01 3:43 AM
Wifi Click have SPWF01S Module. Please let me know how to reduce timing issue.
Is any setting need to do to reduce this or its SPWF01S Module is taking time to send data.
kindly Reply ASAP. It will help us a lot
Thank you
Basavanagouda
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.