2022-07-04 2:12 PM
Hi,
I was looking at the display interface overview and saw that the max resolution for an SPI connection seems to be 480*272.
I'm currently looking at some displays that are SPI 456x456 resolution, so I was wondering if that resolution limitation was in the TouchGFX infrastructure itself or if not, where the bottleneck was.
Thanks!
Daniel
Solved! Go to Solution.
2022-07-05 4:28 AM
Hello DOkaz.1,
There's no resolution limitation from TouchGFX, the document says indeed that the maximum that we could use is 480*272, but that's only recommendation for performances. You can use your 456*456 display if you want but we can't guarantee that the performance would be optimal.
/Osman
2022-07-05 4:28 AM
Hello DOkaz.1,
There's no resolution limitation from TouchGFX, the document says indeed that the maximum that we could use is 480*272, but that's only recommendation for performances. You can use your 456*456 display if you want but we can't guarantee that the performance would be optimal.
/Osman
2022-07-05 12:21 PM
I see, thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.