Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-Cube-AI for BlueNRG-2

Hi,I am using the BlueNRG-2 alone as an MCU.I want to import X-Cube-AI into the BlueNRG-2.However, there isn't the 'BlueNRG-2' name list in the MCU selection in the STM32CubeMX.Is it possible to import the X-Cube-AI into the BlueNRG-2?Thanks

SKim.9 by Associate II
  • 1802 Views
  • 2 replies
  • 0 kudos

DFRO316 MCP3424 and STM32

I am trying to know the status of MCP3424, either it is connected or not to the master STM32 with defined address 0x68. The ADC module gets connected with the Arduino in same address but using STM32, I am not able to get connected with the following ...

PWaiba by Associate II
  • 1182 Views
  • 0 replies
  • 0 kudos

Difficulties in connecting to BLE devices

Hello,I am using a BlueNRG-2 acting as a central to connect with multiple BLE devices, these devices can connect and disconnect multiple times.I am using up to 6 simultaneous connections to different devices, after some successful attempts I keep get...

rsilva by Associate II
  • 8698 Views
  • 15 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.