2018-02-01 10:01 AM
The SPBT3.0DP2 seems to generate its own nReset pulse ocaasionally
The pulse is around 800us
Any reason why this would occur ?
The power supply is stable and the IO is 3.3V
2018-02-01 10:38 AM
Seems to be more reliable when a 10uF capacitor is connected on the +1.8V reg pin (pin 18), but can't say for certain that its fixed it, and its not in the manual
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.