2018-02-13 5:49 AM
Hi,
I have a question about the STEVAL-FKI868V1 development kit that is based on the S2-LP sub 1GHz transceiver. We have a system that works at 868MHz and the signal that commes from the system is fed into multiple TI CC1120 transceivers. The transceivers are configured so that the IQ data is outputed on the GPIO pins from the 1-bit Sigma-Delta ADC. The major problem is that the transceiver don't have a lot of documentation on the subject of extracting the IQ data out of the transceiver so we have faced a lot of issues.
Since we've faced a lot of issues we want to move to other transceivers and looked at the S2-LP transceivers.
In the datasheet we found the following:
The receiver architecture is low-IF conversion, the received RF signal is amplified by a two-stage low-noise amplifier (LNA) and down-converted in quadrature (I and Q) to the intermediate frequency (IF). LNA and IF amplifiers make up the RX front-end (RXFE) and have programmable gain. At IF, the ADCs digitalize the I/Q signals. The demodulated data go to an external MCU either through the 128-byte RX FIFO, readable via SPI, or directly using a programmable GPIO pin.
So therefore the following questions:
Thank you .
#868-mhz #s2-lp2018-05-14 7:38 AM
Hello Winfred
Lu.Winfred
Hope you could reply to this thread.
Basically I also do have same question but on a different EVAL board STEVAL-FKI433V2. In my case I need to receive basicOOK/ASK signal from
https://www.maximintegrated.com/en/products/comms/wireless-rf/MAX14html
.2018-05-14 8:27 PM
Hi Levi, Jismal,
You are probably looking for S2LP's 'Direct through GPIO mode'.
To receive directly through GPIO, please
To transmit directly through GPIO, please
Thank you.
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.