2019-09-24 7:21 PM
I am using NRG-1 for my product development but I have only NRG-2 kit on hand. I am using NRG-2 project to develop my SW for using DK kit but I found there are 250kHz frequency offset when the software is applied to my HW for using NRG-1 inside. Is there any setting to be difference in NRG-1 and NRG-2 in latest 3.1.0 SDK apart from the high clock setting from 16M to 32M?
2019-09-29 6:30 AM
Generally, there shall be no difference in using BluNRG1 or BlueNRG-2. Did you review the tolerance of the XTAL of 16MHz ?
2019-10-02 12:00 AM
Do you mean seeing 250kHz offset for some single tone?
It would be expected behavior.
For stack v2.x, a new parameter, offset, was introduce for ACI_HAL_TONE_START() API for user to start a tone at channel center frequencies without offsets.
Please set the offset to 0.
2019-10-08 12:54 AM
Yes. it is related to 250kHz offset problem. I used command of Radio_Start_tone() in our test code and this 250kHz will be still existed on it so it will give a difference behaviour for using DTM mode vs test code directly.
2019-10-08 6:46 PM
Please get the DTM firmware from the latest SDK, STSW-BLUENRG1-DK v3.1.0 :
https://www.st.com/en/embedded-software/stsw-bluenrg1-dk.html
together with new GUI, STSW-BNRGUI v3.1.0 :
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.