cancel
Showing results for 
Search instead for 
Did you mean: 

Plastic box for STEVAL-BCN002V1B sensortile

NSulj
Associate

Is there any plastic box for  STEVAL-BCN002V1B board. And what is maximum data size which we can sent via bluenrg-2 when BLE characteristic is configured as notify?

Thank you in advance,

Nikola

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

No idea about the plastic box.

BlueNRG-2 supports BLE data length extension, which may have data payload up to 251 byte in one packet.

Decreasing 4-byte L2CAP header and 3-byte ATT Opcode, the maximum length of ATT data can be 244 bytes.

The maximum allowed ATT MTU is 65535, and the maximum characteristics size is 512.

To transmit a characteristics value of length longer than 244, the value has to be fragmented in multiple packets.

However, since notification is a single-packet event, 244 will be its limit.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.