2021-12-15 2:58 AM
Hello everyone,
I am developing a custom board with STM32L4 , and looking to include a "ready-to-use" BLE module, such as BlueNRG-2 series. I have in my possession X-NUCLEO-BNRG2A1 and tested it thoroughly.
In a previous question ( https://community.st.com/s/question/0D53W00001DNzSVSA1/preloaded-firmware-of-bluenrgm2sp ) found out that BlueNRG-M2SP comes "empty" and need flashing with specific firmware before actual use. After searching, I ended up between BlueNRG-2N and BlueNRG-LP processors.
Could you confirm that BlueNRG-2N doesnt need external flashing with firmware (or at least isnt necessary) and can work out of the box ? Is that also the case with BlueNRG-LP ?
Solved! Go to Solution.
2021-12-15 3:07 AM
Hi @path321 ,
Your statement is correct. BlueNRG-2N is already preflashed with DTM image and is so "ready to use". BlueNRG-2N is a chipset (not a module as per blueNRG-M2SP)
BlueNRG-LP is also chipset (BLE SoC) delivered empty.
Regards,
Sebastien.
2021-12-15 3:07 AM
Hi @path321 ,
Your statement is correct. BlueNRG-2N is already preflashed with DTM image and is so "ready to use". BlueNRG-2N is a chipset (not a module as per blueNRG-M2SP)
BlueNRG-LP is also chipset (BLE SoC) delivered empty.
Regards,
Sebastien.
2021-12-15 3:24 AM
Thank you for the support Sebastien.
An additional question, Is ti correct to use the BOM of STEVAL-IDB008V2 as a compass for BlueNRG-2N application circuit described in its datasheet ? Are there any fundamental diffferences between the complimentary parts needed for BlueNRG-2 and BlueNRG-2N chipsets ?
2021-12-15 5:21 AM
Hi @path321 ,
Yes : you are right.
In terms of chipset, BlueNRG-2N is a subset of BlueNRG-2 (some peripherals are not available on BlueNRG-2N). Now, packages are similar, BlueNRG-2 and BlueNRG-2N are pin2 pin compatible.
So, you can use BOM and layout from STEVAL-IDB008V2 - you can also optimize BOM by removing the low speed xTal (32Khz). Default BlueNRg-2N config is using internal low speed oscillator.
As said, BlueNRG-2N is preflashed and can work only in network processor mode (DTM) - not possible to reflash other image than ST ones.
Regards,
Sebastien.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.