2016-11-17 8:38 AM
2016-11-18 12:53 AM
Hi,
which FW versione are you using?That error means that FS image is not sane. Header is not good. Did you use proper tool to create that image?To understand what's happening, can you please try to:- use HTTPDFSWRITE command (update via UART. Do not forget to enable flow control)- use again HTTPDFSUPDATE command, but with a different webserverThis way we can understand if file is sane (and download was not good), or if file is not sane.Thanksjerry2016-11-18 6:42 AM
Hello. I'm using (150410-c2e37a3-SPWF01S) module.
I create this image with gen.bat placed in stsw-idw002.rar downloaded from st.comThere are no HTTPDFSWRITE command description in documents whitch I use (UM1695 User manual. Command set reference guide for ''AT full stack'' for SPWF01Sx series of Wi-Fi modules). So I don't know how to apply correct this command.2016-11-18 6:54 AM
Hi,
that new command has been added to FW3.5.Please update to latest FW release,j2016-11-18 7:41 AM
Could you please point me to where I can get latest firm ware and documentation for newest command set.
2016-11-18 8:38 AM
STSW-WIFI001
For *.11 modules (with embedded 1Mb flash)
http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html
2016-11-21 7:45 AM
2016-11-21 8:24 AM
Cannot write script inside the webserver. All you can do is using what already existing: built-in scripts and SSI mechanism. Please take a look at AN4902
: SPWF01Sx – dynamic web pages (http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html)
Regardsjerry2017-06-15 11:44 AM
Hello. I used html code from '
SPWF01Sx – dynamic web pages' Output demo – multiple text boxes with script which allows skipping the automatic redirect. But after pressing submit button it redirect to output_demo.html. Why?
2017-06-15 6:16 PM
Because it's built on top of HTTP GET request. Request for some html resource. Which one? That one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.