2021-03-15 11:07 AM
I have seen some thread about this topic but it's still not clear to me.
I'm using the x-nucleo-BNRG2A1 which embed a BNRG-M2SP. Is it possible to increase the ATT_MTU size ? for example in the sample example code we do a aci_gatt_exchange_config(connection_handle) but there is no way to change or initialize the ATT_MTU size.
same thing with the BLUENRG-M0A which is 4.2 compliant.
Regards,
2021-03-15 7:22 PM
Set the attMtu parameter during initialization when calling BlueNRG_Stack_Initialization().
GATT exchanging for MTU is still required, since the ATT MTU is a negotiated value.
2021-03-16 2:55 AM
Thanks for your reply, But I'm currently running the X-cube-BLE2 examples code (version 3.2.0) and there is no BlueNRG_Stack_Initialization() function.
Can you point me to the right API to use?
Indeed the MTU is a negotiated value that's why I try to pair two x-nucleo-BNRG2A1 or using the sample App on an iPhone
Regards
2023-02-28 1:52 AM
Any response here?
2024-08-29 4:46 AM
Did you ever find the solution for this? I'm stuck in the exact same shortcoming.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.