2021-10-27 6:29 PM
The pins with red boxes are supposed to be OUT pins as indicated on the datasheet. (see picture). However, the actual layout looks like the GROUND pins. I am not sure if i am seeing it right, someone pls help! Thank you.
Solved! Go to Solution.
2021-10-27 11:59 PM
Welcome, @Klim.1, to the ciommunity!
You didn't write which component you were talking about, but it's either VNH7070 or VNH7100.
The pins marked in red are clearly the outputs of the half bridges, as can also be seen in the datasheets, Fig. 15. The GND pins are in exactly the right place (pin 1, 8, 9, 16) and are connected to the sources of the low-side FETs (top and bottom die). A recommended layout is shown in Fig. 17 of the datasheet.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-10-27 11:59 PM
Welcome, @Klim.1, to the ciommunity!
You didn't write which component you were talking about, but it's either VNH7070 or VNH7100.
The pins marked in red are clearly the outputs of the half bridges, as can also be seen in the datasheets, Fig. 15. The GND pins are in exactly the right place (pin 1, 8, 9, 16) and are connected to the sources of the low-side FETs (top and bottom die). A recommended layout is shown in Fig. 17 of the datasheet.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-10-28 12:04 AM
Thank you peter. Yes it's for VNH7100
Your answer is clear. Apprecaite it!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.