Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
If changed char length 450 to 140 now every thing will be fine. but when i put char length 450 or more than 140. It will return 0x48 error value.The paramerters i was passed, these are ret = aci_gatt_add_char(chatServHandle, UUID_TYPE_128, (Char_UU...
I am designing some firmware for a BlueNRG LP (355MC) based device with several sensors. At certain points in the device's processing/lifecycle, I need to turn off the BLE and/or radio to conserve power. In fact, I only need the device to have BLE co...
Now and again, following power-up, we find the STS1TX in our product in a state where we cannot interface with it. The SPI and GPIO lines are outputting ~2V levels, so no commands can be sent.Typically, cycling power may allow the chip to initialise ...
Very standard "app note" circuitGood decoupling. 2.8v switched supply railXO is up within 350uS of startupDevice is programmed about 100uS after detection of the "reset OK" state
Hello,I'm doing some development work with an STEVAL-IDB011V1 dev board. I'm targeting very low power and so I would like to verify the numbers listed in the datasheet.In DEEPSTOP mode at room temperature, I am expecting something around1 μA of suppl...
I am trying to acheive a BLE Mesh system where no network data will be stored to NVM, i.e. system will need to reconfigure on every reset.The network consist of one PRV and a handfull of LPNs, the LPNs will be mobile and will therefore enter and leav...
hi,I am trying to transmit at maximum power using S2-LP. I set the configuration registers using S2-LP DK Application tool version 1.3.4. I set output power as 14dBm, check the MAX power box, choose HPM mode (in PM mode section), set 1600mV SMPS volt...
Hello,https://www.st.com/content/dam/OLM%20Email%20Marketing/2021/EMEA/Events/BlueNRG-LP/STBLEBlueNRGLPWebinarApril20V3.pdfIn page 9 of the above document STM is mentioning FFT - my question is - where can I find libraries for FFT, FIR etc. for Blue...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.