2021-10-19 5:49 AM
Hi,
I just got a STEVAL-IDB008v2 boards and I want to test lighting demo example available in STSW-BNRG-Mesh. I have followed the steps in "Getting started with the ST BlueNRG-Mesh embedded firmware". Unfortunately, there is error while building the program using Keil:
error: L6050U: The code size of this image (174134 bytes) exceeds the maximum allowed for this version of the linker.
Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.
Target not created.
I got similar error when I tried to use IAR. Any advice how to resolve this issue?
Thank you in advance!
2021-10-21 8:59 AM
Hi,
As per the error: L6050U: The code size of this image (174134 bytes) exceeds the maximum allowed for this version of the linker.
It seems, IAR & KEIL are able to compile the code only up to 64K due to license unavailability.
For IAR: Time limiting option can be selected through which code of any size can be compiled but only for 30 days.
Whereas for KEIL: Free license is available for STM32F0/G0/L0 and BlueNRG-1/2/LP and more details are available on the link shared below:
MDK for STM32F0/G0/L0 and BlueNRG-1/2/LP - Installation & Activation (keil.com)
2021-10-21 12:41 PM
Thanks for your quick response. This helped me a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.