Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm developing a very simple product using BLUENRG-232N. I was wondering, whether this device can function as an SPI master to just read some data from sensors, and send it over BLE ?

I'm developing a very simple product using BLUENRG-232N. I was wondering, whether this device can function as an SPI master to just read some data from sensors, and send it over BLE ?​The documentation is also pretty confusing. It says that there are...

DBasu.1 by Associate
  • 728 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-BNRG2A1 and Arduino

I want to use the BNRG-MS2P of this module with an Arduino. More specific with a custom PCB with an atmega328p. Any tutorial, Literature I can use. This is a new field for me

Pgonz.1 by Associate II
  • 809 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-BNRG2A1

Hi,I have a project that needs BLE connection. Right now I have a custom PCB working with a premade BLE module (SH-HC-08), the PCB has an atmega328p. Now is the time to upgrade with a custom BLE chip for creating my own characteristics.For this, I st...

Pgonz.1 by Associate II
  • 682 Views
  • 0 replies
  • 0 kudos

STCUBEMX code generation missing some pins?

So I'm new to the stm32 line up and I'm currently trying out the STCUBEMX code generator. After generating the code, I can't seem to find the configurations for the pins I selected. For example, I chose PD5 and PD6 as TX and RX for USART2. But when I...

SYes.1 by Associate
  • 1485 Views
  • 1 replies
  • 0 kudos

ADC pin current requirements?

I'm designing a guitar pedal using my F767ZI Nucleo, and I have an input stage current buffer using a TL072 op amp. I'm using the Nucleo's 3.3v as VCC.I would like to know if I can wire the op amp output pin directly to the ADC pin on the Nucleo, or ...

NNagy.1 by Senior
  • 1036 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.