2019-05-13 12:46 PM
Hi,
I'm using the example "BLE_SensorDemo_Central" from SDK to design a PoC to scan iBeacons devices.
I can't figure out why the scan procedure is too slow.
I have two iBeacon devices near by the BlueNRG-1.
They are sending iBeacon messages in 3Hz, but the BlueNRG is not fast enough to get the packages.
What am I doing wrong?
I understood that the method "Master_DeviceDiscovery()" set the scan parameters, right? I couldn't find on documentation the min or max for scan interval or scan window.
What do I need to do to get best performance from BlueNRG-1 on scan mode? I don't need to connect, just get the iBeacon messages.
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.