2022-03-25 7:02 PM
2022-03-28 2:02 AM
Hi @Fx.1 ,
Let me share with you PM0269 document : This is BLE Stack Programming guide.
You may refer to section 3.1.1 describing Bluetooth LE addresses managment.
The BlueNRG-LP device does not have a valid preassigned MAC address, but a unique serial number (read only for the user).The unique serial number is a 8-bytes value stored at address 0x10001EF0: it is stored as two words at address 0x10001EF0 and 0x10001EF4.
If you want to use static random adress : this address is generated and programmed at very 1st boot. This address is used and remains unchanged during whole product life (except is a mass erase of the flash is performed)
Regards,
Sebastien.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.