cancel
Showing results for 
Search instead for 
Did you mean: 

Glue which contains phthalates is used in IC. Percentage of phthalates (DBP) is exceeded allowed threshold level stipulated by EU RoHS directive. - Does the DBP evaporate during manufacturing process?

ADres.2
Associate

Hi, I got material compliance from Silicon Expert Database. Concerned part is an IC. According to Silicon Expert, there is glue used for die attach. The glue contains a phthalate based substance, DBP. DBP use is restricted by EU RoHS directive, via delegated directive 2015/863. There shall be not more than 0,1% w/w of this phthalate in homogenous material in an EEE (i. e. in the IC which is integrated into an EEE). Problem: the glue contains more DBP than allowed by EU RoHS directive. It´s about 0,2 %, not 0,1 %. Actually, it´s mikrograms per IC. But it is exceeding the threshold. - QUESTION: What happens with DBP in such glue? Does it evaporate when the glue material hardens? I. e. is there no DBP remains in the IC when it is distributed? - I am grateful for helpful hints.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.