2022-11-24 2:07 AM
2022-11-24 2:52 AM
Welcome, @MM.25, to the community!
The KS8721CL is or was a PHY for 10BASE-T, 100BASE-TX and 100BASEFX, which STMicroelectronics does not have in its portfolio. However, maybe one of the users in the community has a recommendation for you.
Good luck!
/Peter
2022-11-24 2:55 AM
Thank you peter
2022-11-24 2:57 AM
You're welcome!
If the problem is solved at some point, please mark this thread as answered by selecting Select as best for the relevant answer, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2022-11-24 2:22 PM
You are asking for alternates, but have not named a single requirement and have not even told what exactly you mean by "alternate". With such amount of information I can recommend DP83561.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.