2018-03-22 1:56 PM
Hi,
We are evaluating the use of the BT Module SPBT3.0DP1 on one of our devices.We are trying to configure the PIN to connect to a legacy device, that already has a predetermined PIN code that uses letters (lower and upper case)Unfortunately, the current Firmware on the module cannot setup capital letters as PIN for Bluetooth pairing on SPBT3.0DP1 BT Mod. The current firmware converts all letters to lower case, and therefore, the PIN doesn't match and cannot connect to the legacy device. See commands and responses below.at+ab build
AT-AB DataPackage FW Build 170925 - 1.1.337at+ab config pin=1234AT-AB ConfigOKat+ab config pinvar6 PIN = 1234at+ab config pin=lowercaseAT-AB ConfigOKat+ab config pinvar6 PIN = lowercaseat+ab config pin=UPPERCASEAT-AB ConfigOKat+ab config pinvar6 PIN =uppercase
at+ab config pin=MIXEDlettersAT-AB ConfigOKat+ab config pinvar6 PIN =mixedletters
at+ab resetAT-AB ResetPendingAT-AB -CommandMode-AT-AB BDAddress 0080e1ba01c2at+ab config pinvar6 PIN = mixedlettersWe have the following questions:1. Do you have a newer firmware version for this module that fixes this issue?2. If not, how long would it take to generate a new version of firmware to correct this issue?3. Is there a workaround that could be used to program the correct PIN for BT pairing?
Regards,Alex R.#pin #bluetooth #stbp3.0dp1 #moduleWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.