2025-05-19 8:43 PM - last edited on 2025-05-22 4:32 AM by Andrew Neil
Hello,
I'm using STEVAL-IDB011V2. From the BlueNRG-LP Navigator, I can load the examples on the board. But when I'm using the Keil, it says "SWD/JTAG Communication Failure".
On the options for target in the tab "Device" the device is BlueNRG-355, and the Software Pack is "Keil.STBlueNRG-LP_DFP.2.0.0". In the tab "Debug" it uses "CMSIS-DAP Debugger".
Cannot erase the code either. Jumpers J3-J5 are all in place and not faulty.
SW device error. Not sure what else to try. Thanks heaps
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.