2026-01-16 5:48 AM - last edited on 2026-01-16 6:31 AM by Andrew Neil
Hi STM team,
I would like to know if/how I can simply connect e.g. the ST67W611M1 or another WiFi module to a switch IC, e.g. the KSZ8795CLXIC, without needing a microcontroller. Or is there a switch IC that can be connected directly to the ST67W611M1, e.g. with SPI?
If possible, do you have an application, a sample circuit or a development board for me?
Thanks in advance!
Best regards,
Christos
2026-01-16 6:29 AM - edited 2026-01-16 6:32 AM
The ST67W611M1 is not a standalone solution - it requires a Host processor.
I asked the question here; the answer is here.
Note that KSZ8795CLXIC is a Microchip product - nothing to do with ST - so you'd have to ask Microchip about that.
Its SPI is for configuring the switch itself - not for the switch to configure a WiFi module (or anything else).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.