2019-12-18 8:14 AM
Hello,
I'm designing a custom PCB with STM32L476RG. I need to add Bluetooth 5 connectivity. I'm looking for a BT module with the following requirements:
Is there a recommended module?
Thanks in advance
2020-01-08 7:58 PM
Hi bro, few notes:
"Transmit at least 2Mbps" - 2M is a PHY layer speed so real data throughput is less (1-1.5 Mbps max). May be it is a good idea to use Wi-Fi for your application if more speed is needed
"As small as possible" - if dimensions are critical you can use SoC with MCU+BLE in 1 IC
"..compatible with the above MCU.." it's no problem, because every module supports UART, SPI
You can look at the SaBLE-x-R2, I worked with it, it's decent BLE5 module
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.