2021-01-05 8:50 AM
Hello everybody,
I plan to add an bluetooth chip to my electronics board. My goal is to add a basic bluetooth serial communication, in order to send errors messages to an android app.
I use STM32 microcontrollers on my boards, and I program them with STM32Cube IDE.
As I need something very basic and simple, I'm trying to choose the easiest chip, and I think the BlueNRG-MS seems to be the most "easy" to use since it embeds all the bluetooth stacks in it ! What do you think ?
I didn't find any library for STM32Cube IDE, I think I will have to create it ?
If you have any advice, I take it ;)
Thanks for reading,
Best regards
Valentin
2021-01-11 9:36 PM
BlueNRG-MS is a BLE tranceiver, which shall be simpler than BlueNRG-1/2/LP SoCs (MCU + BLE transceiver).
The X-CUBE-BLE1 expansion software package for STM32Cube can be used for your reference:
2021-01-12 5:47 AM
Thanks for the information.
I bought the X-NUCLEO-BNRG2A1 board, which is working with a BlueNRG-M2. I'll start with this one, while keeping in mind that BlueNRG-MS would be easier.
2021-01-12 5:24 PM
BlueNRG-2/M2 can be programmed so that the embedded Cortex M0 takes care of BLE stack tasks only.
This way it can act exactly the same way as a BlueNRG-MS.
Please refer to DT0121:
DT0121 How to configure the BlueNRG-1 and BlueNRG-2 devices in network coprocessor mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.