2015-01-28 2:22 PM
Hello, I have few questions:
1. Can BlueNRG or BlueNRG MS function as a Central and peripheral role at the same time?2. Can BlueNRG or BlueNRG MS function as a Central and broadcaster role simultaneously?3. Can a BlueNRG central device perform discovery of new peripheral devices while connected to 3 other peripheral devices? Thanks. #bluenrg2015-03-17 7:11 AM
Hi,
using the BlueNRG-MS, you can configure all roles (Peripheral|Broadcaster|Central|Observer), while using the BlueNRG you can configure only one role between Peripheral, Broadcaster, Central and Observer.
Using the BlueNRG device, you cannot perform a discovery procedure while the device is already connected with other devices.
Regards,
GraziellaHello, I have few questions:
1. Can BlueNRG or BlueNRG MS function as a Central and peripheral role at the same time? 2. Can BlueNRG or BlueNRG MS function as a Central and broadcaster role simultaneously? 3. Can a BlueNRG central device perform discovery of new peripheral devices while connected to 3 other peripheral devices? Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.