2017-04-12 11:48 AM
Hi,
I have noticed that it is not possible to have multiple ACI_GATT_WRITE_CHAR_VALUE per connection event.
I have set up the following connection: connection interval of 40ms and connection event length of 21.875ms (the maximum I can while continuing to advertise in parallel).
Using a sniffing tool, I see that what is happening is the following:
- Master -> Slave : Write Request
- Wait for 40ms (next connection interval)
- Slave -> Master : Write Response
- Wait for 40ms (next connection interval)
- Master -> Slave : Write Request
- etc.
Is that a normal behavior? Why isn't it possible to have the Write response inside the same connection event, and more write reqests?
Note that if I use ACI_GATT_WRITE_WITHOUT_RESP (Write command), I don't face the issue, and it's possible to send multiple ones inside the same connection event (around every 700us)
Thanks for your help.
Christian
#bluenrg-msSolved! Go to Solution.
2017-04-19 1:42 AM
Hi Christian,
yes, it is an expected behavior since the slave will wait for its own connection interval to send the response required by the ACI_GATT_WRITE_CHAR_VALUE.
Kind regards
Andrea
2017-04-19 1:42 AM
Hi Christian,
yes, it is an expected behavior since the slave will wait for its own connection interval to send the response required by the ACI_GATT_WRITE_CHAR_VALUE.
Kind regards
Andrea
2017-04-26 1:55 PM
For my education, would you mind pointing me to the reference in the Bluetooth CORE Specifications?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.