2017-02-21 12:57 PM
Hello, I am using a BlueNRG-ms (IDB05A1) flashed to latest fw 7.2c trying to develop a HID compliant mouse for Windows.
However when pairing with windows using only the basic GATT and GAP(no other services or changes) from the BlueNRG GUI there are some problems, Windows says:
Device (0x280E1003C2A) is not Compliant with the Bluetooth Core Specification: previous attribute was a (Characteristic), current attribute is a (Descriptor).
Is this a bug or is Windows wrong? BlueNRG-ms page states:
'
The BlueNRG-MS is a very low power Bluetooth low energy (BLE) single-mode network processor, compliant with Bluetooth specification v4.1.'
Is this a cause for concern?
#stm32 #bluenrg-ms #windows #idb05a1 #hid #bluetooth #ble2017-02-22 6:41 AM
bump
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.