2018-07-09 5:13 AM
Hello all,
I am using the DTM for bluenrg-1 I can program the unit and it will work fine but for some reason when the unit is left powered down for a couple of hours and then powered up again some times stops working.
Doing a flash reading starting in address 0x10040000
I can see the next difference:On the unit that is working:
00
60
00 20 61 16 04 10 29 18 04 10 39 18 04 10On the unit that stops working:
00
00
00 20 61 16 04 10 29 18 04 10 39 18 04 10For some reason that byte changes value.
Any idea why that problem could happen.
Thank you
2018-09-14 2:43 AM
I have seen a different problem, the bluenrg-1 was working fine pairing and communicating with other devices, then I powered down for a time and next time I power up the unit didn't work.
Reading some locations from flash I can see that they are 0xff somehow the flash got corrupted/blank.
Someone has seen that problem before.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.