2017-02-23 5:49 AM
Hi everyone, I want to implement a very simple file transfer via BLE from my SensorTile to a remote device.
I need to edit the BlueMicrosystem2 V2.2.0 firmware in order to add a new characteristic: such a
characteristic should read a file from the SD card and send them from the SensorTile to the remote device (a kind of reverse FOTA).
Reading the file is not a problem, but I have no idea where to start from for developing the service which provides this file upload
characteristic.
Can you point out a code snippet or where, in the firmware code, there is a similar GATT service that may be adapted easily to me needs.
Tnx!
Andrea
#ble #bluenrg #sensor-tileWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.