Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello,I'm using The BlueNRG-M2SP with the x-nucleo-BNRG2A1, and I wan't to send and receive ascii and hex, from the ble to my phone using "UART". I wan't to know if there is an example to use for this situation with or without flashing the BLE, Regards,

I'm using : the X-Nucleo-bnrg2A1A nucleo L476RGand I already tried to Flash my bluetooth with the examples on the firmware ST BLUENRG DK, especially the DTM. And tried the BLE_chat but I can't see the bluetooth in my phone using BLE Scanner.

abach.1 by Associate II
  • 4258 Views
  • 8 replies
  • 1 kudos

Bluenrg-m2 SPI interface with stm32f103

#BlueNRG​  #STM32WB​ #BLE​ #[BLE Mesh]​ #[STM32 MCUs]​ #STM32F1​ I'm interfacing bluenrg-2m When I reset the reset pin, the bluenrg-2m set the boot pin to high, and this correspond to the external interrupt of mcu and this work successfully.The exter...

Advertising table problem

Hello,I am working on a BLE project and I have a prolem of advertising table.- when I try to fill the advertisement table and I want to add more information, I don't see all the advertisements on the application, and I see the arbitrary information,...

AMACH.1 by Associate II
  • 1264 Views
  • 0 replies
  • 0 kudos

BlueNRG Windows connection problem

Greetings, fellow community members,I am currently utilizing the X-NUCLEO-IDB05A2 board and have configured the Bluetooth module using the BlueNRG GUI.The module establishes a successful connection with an Android phone without any issues. However, w...

MCift.1 by Associate
  • 1044 Views
  • 0 replies
  • 0 kudos

Avaialability of xt2046 based touch ic library

Hii everyone,i am working with a 2.8 inch spi display, using ili9341 display driver, adn it is having xt2046 touch driver on it.Can anyone please guide me for the right and stable library available for using xt2046..i am unable to find any

skuma.8 by Associate III
  • 2386 Views
  • 4 replies
  • 0 kudos

Alternatives to TC2030 tag connectors

What kind of connectors do you use, when there's no space for soldered connectors for flashing your boards?I wonder if there's a wider distributed (and cheaper) solution than TC2030-nl connectors. Those are nice, but waaaaaaay too expensive.

MWebe.3 by Associate
  • 1230 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.