Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in the BLESensor-App(X-Nucleo-BNRG2A1)

Hello, i used the CubeMX to generate the example code for the X-Nucleo-BNRG2A1 board. The Example works well when the #define USE_BUTTON (0) :  However, when #define USE_BUTTON (1) I get the following blank page:  I've had the same behavior before up...

AElgh_0-1706898887202.png AElgh_2-1706898956139.png
AElgh by Associate III
  • 873 Views
  • 0 replies
  • 0 kudos

STUSB1600 NVM re-programming

Hi,How do you re-program the NVM on STUSB1600? The current datasheet (DS11503 - Rev 4) refers to Chapter 6 that doesn't give any information.Best regardsNiclas

NArnd by Associate III
  • 3434 Views
  • 4 replies
  • 3 kudos

STUSB1600A can't switch to Source

I have STEVAL-CCC002V1 with STUSB1600A controled with STM32F103 over I2C. Samsung Galaxy Tab connected to USB-C and I want to charge it.But I can't switch to "source power role". No matter how hard I try the controller is still in sink.Here I have a ...

20240131_125212.jpg
riske by Associate II
  • 970 Views
  • 0 replies
  • 0 kudos

L9663

Mode 2 Can read and write sensor data directly through the psi5 operation register?

JL1 by Associate II
  • 751 Views
  • 0 replies
  • 0 kudos

L9663

Can Mode 2 of the L9663 read the sensor data directly with the MCU? Or do we go through SPI?

JL1 by Associate II
  • 778 Views
  • 0 replies
  • 0 kudos

a problem about BLE_HID_Peripheral

I am using the blue-nrg-lps,but when i test the hid example project , it cannot work in win11,but it is ok in phone and pad,so anyone can tell me why? A new player of ble-nrg-lps...

yyys by Associate II
  • 641 Views
  • 0 replies
  • 0 kudos

BLUENRG-LP BLE HID KEYBOARD with WINDOWS 10 PC

DK version:BlueNRG-LP DK 1.1.0chip:BlueNRG-345AC​2 problems of the ble hid keyboard project. ​1st, if BlueNRG-LP is not conneted to any device,it keeps going into RESET ,go on and go on.when it connected to one device,this situation stoped.​2nd,BlueN...

WYuan.1 by Associate II
  • 3056 Views
  • 4 replies
  • 0 kudos

BlueNRG-LP: Flash controller mass erase command?

Hi All,In the reference manual for the BlueNRG-LP Cortex M0+ microcontroller (RM0479), it states both page and mass erase functionality for the flash controller. But, only one "ERASE" command is given (0x11), which appears to be for page erase.Does a...

PStinson by Associate II
  • 4420 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.