Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Spirit1 stuck in PM_setup state (0x3B)

Posted on November 26, 2014 at 17:56 Hello, I try to set up a spirit1 device. I use your given Spiriti1 library and the example projects, but while radiInit, my device stuck everytime on the same point: SpiritCmdStrobeLockTx()...

steport by Associate II
  • 2754 Views
  • 8 replies
  • 0 kudos

BlueNRG indication issue

Posted on October 13, 2014 at 10:33HelloI have the following issue with BlueNRG: when I try to use ''INDICATION'' to sending data from server to client I have ble crash (the BlueNRG stops to respond to any command) after a few indicate packet (50 - ...

Please provide descriptions of the ACI calls:

Posted on November 25, 2014 at 17:00Dear ST The application command interface (ACI )document UM1755 is incomplete. Many of the calls don't list the parameters to pass, and the results returned. In some cases it is possible to find this information f...

charles23 by Associate III
  • 1030 Views
  • 1 replies
  • 0 kudos

SPWF01S information

Posted on November 25, 2014 at 17:23I need some information about this WiFi Module, I've already read theonline doc but I haven't found all the information I need.1) I see the module use Uart1 to communicate with host, with hardware control, but I c...

dynamic pages and file .cgi

Posted on October 21, 2014 at 09:20Hello,In the module spwf01sa there are already some interfaces .cgi, but how can I add new ones? With the the AT+FSC and AT+FSA commands? Or  there is another method?

l2399 by Associate
  • 1403 Views
  • 5 replies
  • 0 kudos

BlueNRG International Availability

Posted on April 08, 2014 at 23:21Does anyone have any information about why these parts are restricted outside the US? We have been trying to order the dev kit and some samples to New Zealand for several months now, and both DigiKey and Mouser state...

stefel by Associate II
  • 2486 Views
  • 5 replies
  • 0 kudos

SPWF01SA HTTP Request

Posted on November 19, 2014 at 14:43Hello everybody!It is interesting to me to make an electronic device which can receive data from the mobile devices (e.g. Mobile Phone or Computer). The main idea is to send data to electronic device by using the ...

Roma Jam by Associate II
  • 2818 Views
  • 11 replies
  • 0 kudos

STEVAL-IDW001V1 documentation?

Posted on April 28, 2014 at 16:28Hi, I just received a STEVAL-IDW001V1 eval module.  It is meant to connect to a Discovery F0 board, but intend on using it with a STM32F215 processor based device.  I haven't found much documentation about this eval ...

vneff by Associate III
  • 902 Views
  • 3 replies
  • 0 kudos

can not customize WPA mode (Mini AP).

Posted on November 12, 2014 at 20:03Software SPWF01S-140805-3f58d6b-RELEASE-mainSet Mini AP mode: ---------------------------------------AT+S.SSIDTXT=MY    (get/set a textual SSID)AT+S.SCFG=wifi_wpa_psk_text,SUPER  (WPA(2) PSK passphrase, if set the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.