Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the Max Read/Write Buffer Sizes for BlueNRG

Posted on March 23, 2015 at 22:50Hi- Doc UM1755 says slave header on SPI indicates read/write buffer size by bytes 1-2 and 3-4. If ACI command pkt is bigger than 128 bytes then mast has to send it in 2 SPI write transactions. Does it mean the size f...

hui by Associate II
  • 1153 Views
  • 1 replies
  • 0 kudos

hci_le_transmitter_test is working well?

Posted on March 25, 2015 at 16:15Hello, Can you clarify how work function hci_le_transmitter_test?I could not find any description of this method. I found that the test run for just a second, but I thought that the test will continue until the comma...

How to enable FEC on Spirit1

Posted on March 10, 2015 at 08:39Hello,I have Spirit1 IKR02v3.0 development kit. It contains an STM32L151 MCU and Spirit1 RF module. But I use Spirit1 with STM32L162RD MCU for a project. I created my own project on Keil. I ported all the spirit1 fir...

hacer by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos

Headers and APIs for SPIRIT1 on TI-ARM

Posted on March 17, 2015 at 19:27Hi,I have a TI tm4c123gh6pm microcontroller and would like to use the SPIRIT1 with it. Are there integrated API's and functions that I can directly include for a faster implementation, compatible with this controller...

Flash recovery

Posted on August 11, 2014 at 11:24Hi,I'm developing a device based on the BlueNRG. I worked on the support of flash BlueNRG from my firmware,  but during a flash error occurred (probably due to an incorrect program address). After flash failed BlueN...

How to set a specific channel for advertising?

Posted on March 27, 2015 at 12:23Hello, Please, help me to clarify the following question: Can I set one specific channel for advertising (37 channel for example)? I have tried to use hci_le_set_advertising_parameters function, but to no avail! Re...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.