Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01xx more info on TLS handling?

Posted on October 28, 2016 at 01:38HelloI'm evaluating the SPWF01SA for an industrial application especially with regard to its TLS capabilities.Unfortunately my knowledge of TLS especially in an embedded setting is limited, and AN4683 neglects to m...

SPIRIT1 RSSI Filter Gain

Posted on October 19, 2016 at 15:46Hi,I am doing some measurements using the RSSI from the SPIRIT1. I am making the the following test:In the transmiter I am using the continuos wave In the receiver I am verifing the RSSI as the following:Enter RX s...

Saving Settings Without Damaging Flash

Posted on October 13, 2016 at 21:18Hi guys,SPWF01S is a new module for me.  I have been using it for about a month.My question is this: if I set the WiFi connection options at every boot and issue an AT&W (save), will it wear out the eprom memory?  ...

SPWF01S Test mode

Posted on October 18, 2016 at 14:17Hi, UM1695 mentions that there is a special test mode that is enabled via configuration variable ''eft_mode''. Description says ''Enable/disable the Engineering Test Functions. It is used for controlling the radio ...

jarno2 by Associate II
  • 828 Views
  • 1 replies
  • 0 kudos

Unavailable programming manual??

Posted on October 03, 2016 at 13:49Dear all,I have already posted /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Where%20to%20find%20a%20programming%20manual&FolderCTID...

Command Mode for Server Socket

Posted on October 14, 2016 at 23:55I have a server socket that automatically goes into data mode when a client connects.I would like to be able to go back to command mode by using the escape sequence ''at+s.'', but it doesn't work, even if I set a c...

spirit1 autoack problem

Posted on October 06, 2016 at 11:35We are testing p2p connectivity software on NUCLEO L152RE + X-NUCLEO-IDS01A4. We need to use auto acknowledgement and auto retransmission feature on spirit1. Whatever the application in the SUBG1 package, is not us...

vamsi by Associate II
  • 696 Views
  • 0 replies
  • 0 kudos

Spirit1 / SPSGRF receive

Posted on October 04, 2016 at 16:58Hi,I use the SPSGRF module in 868MHz Narrowband. I search to send packet with this configurations : - Fc = 869.2375MHz- Fdev = 2.7 kHz- Datarate = 4.8 kBit/s- Number of channels : 0- Spacing channel : don't care ? ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.