Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLUENRG-1 standalone

Posted on March 30, 2017 at 13:05Hi All,I have question about BLUENRG-1, can it run as stand alone without another MCU?If yes, I would appreciate very much if you could refer me to some references.Regards,Nav Dev.#bluenrg-1 #standalone-mode

Nav Dev by Associate II
  • 2380 Views
  • 4 replies
  • 0 kudos

SPWF01SA WIFI MODULE SEND INFORMATION TO UART,

Posted on March 31, 2017 at 13:29Hi All, I need to send information using the uart of my SPWF01SA wifi module. I have seen that uI need to use the signal TXD1 but i dont know if it is possible send data to this signal using http.I have made some tes...

GAR Gar by Associate
  • 1387 Views
  • 3 replies
  • 0 kudos

Firmware for BlueNRG-MS

Posted on March 30, 2017 at 18:34I am communicating with the BlueNRG-MS over SPI using an ST eval board with an F1 micro. I am able to send data over the MOSI line and receive the 0x2 ready data as shown in the attached image. I am having issues wit...

daithi62 by Associate II
  • 1601 Views
  • 2 replies
  • 0 kudos

SPWF01SA.21 WiFi Module

Posted on March 28, 2017 at 17:17Is it possible to connect an external eeprom to the SPWF01SA.21 module? The stored eeprom data will be very small >1K and only serve to remember GPIO high or low settings of the modules STM32F103 core that an end use...

New to BlueNRG-1!

Posted on February 24, 2017 at 07:37Hi, I am new to ST-Bluetooth. I have experience in TI LPRF and planning to do something in BlueNRG-1, because of TI background I have few questions! TI BLE stack is based on IAR/CCS IDEs, for ST stack what is the...

pradeesh by Associate
  • 934 Views
  • 1 replies
  • 0 kudos

How to test IPM

Posted on March 31, 2017 at 02:45I purchased IPM for my degree project with parts number: STGIPS20C60 and it is connected with the PWM and the IPM is not working . I want to test the IPM any idea  how to test if the ipm is working or not. 

Sensortile BlueNRG-MS Custom Service ACI

Posted on February 28, 2017 at 16:19Hi,I am working on Sensortile kit with the BlueNRG-MS radio.As per ST document PM0237 section 3.3, pg 55/99, following commands are used to add custom service to BLE device : //Add the service with service_uuid 12...

RADS1 by Associate II
  • 4396 Views
  • 7 replies
  • 0 kudos

Spriti1 application

Posted on March 23, 2017 at 17:03Hello everybody,I have the STEVAL-IKR001Vx evaluation kit and the SDK-2.0.1 and SDK-2.2.0. I have been trying to work with the GenericBasic_A and B. Both files compiled without any error in IAR and Keil v4. However, ...

idris by Associate II
  • 655 Views
  • 0 replies
  • 0 kudos

Spirit1

Posted on March 23, 2017 at 16:47Hello everybodI have the STEVAL-IKR002Vx developmental kits and downloaded the SDK 2.0.1 and 2.2.0. I have been working on the SDK_BasicGeneric_A and B. The code compile fine in both IAR and KeilV4. However, nothing ...

idris by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.