Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BlueNRG-1 extended packet length

Posted on October 05, 2017 at 10:47I am evaluating the use of the SPBTLE-1S module, based on BlueNRG-1 and Bluetooth v4.2 compilant, to interact with iOS. BLE 4.2 specification includes data length extension feature which improves throughput and red...

BlueNRG

Posted on October 09, 2017 at 11:42Hello All, i want to modify the application on the Details Activity class. I want there to change the temperature into weight because i would like to make some messurements with some resistive wire strains. So did ...

SP1ML module with low distance range

Posted on October 06, 2017 at 15:49Hello,   I'm working on a project, where I need RF transceivers. I chose Your SP1ML transceiver modules, but I was dissapointed when I tried the devices, because the low distance range. The distance range abaout 20...

SPWF01SA - Setting the IP Address

Posted on October 04, 2017 at 14:34Hi,I have recently just started working on Wi-Fi code on the SPWF01SA module using the STM32F1 Nucleo Development Board.I was able to get the various configuration values from the Wi-Fi module using the functions b...

0690X00000608TUQAY.png 0690X00000608N9QAI.png

SPI2 not working in stm32f070

Posted on October 04, 2017 at 07:37Hello Allcurrently i am working in Fatfs with stm32f070 with spi1. when i move to spi2 its not working. i am trying multiple times but i cant get success. here is my init functionvoid SPIFlashInit(void) { SPI_InitT...

Build OTA in Sigfox project on BlueNRG1

Posted on October 02, 2017 at 04:56Hi,I tried to add OTA function in BLE_SigFox_SensorDemo project,and according to OTA guide, I have to add, ST_OTA_LOWER_APPLICATION=1 or ST_OTA_HIGHER_APPLICATION=1 as preprocessor and linker options.After adding S...

Wei Lu by Associate
  • 782 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.